Search
Languages

Bourns Expands Line of Riedon™ Industrial Shunt Resistors with Six New Model Types

New models deliver superior current handling capabilities to meet accurate measurement requirements in applications ranging from renewable energy to industrial power systems

RIVERSIDE, Calif., August 26, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the expansion of its line of Riedon™ Industrial Shunt Resistors with the release of six new model types. The new shunt resistors feature superior current handling capabilities that meet accurate current measurement requirements. Precise measurements are necessary in a wide range of applications including battery management systems (BMS), solar inverters, welding equipment, heat-treating equipment, battery chargers, power supplies, cathodic protection rectifiers, and marine and mobile accessories.

The new industrial shunt resistor models are available with panel and busbar mounting options. The Riedon™ Model RSN and RS Series shunts by Bourns are panel mount products with a current handling capacity from 1 A to 1200 A, resistance values from 0.0417 milliohms to 100 milliohms and tolerances from 0.25 percent to 1 percent. The Riedon™ Model RSH, RSI, RSJ, and RSW Series shunts by Bourns are designed for direct mounting to busbars with a current capacity from 5 A to 6000 A, resistance values from 0.025 milliohms to 10 milliohms and tolerances of 0.25 percent.

All Riedon™ industrial shunt resistors by Bourns are precision shunts that incorporate low-resistance Manganin™ as their resistive material. These new shunts also offer a wide operating temperature range of -40 °C to +80 °C, and feature a compact size and center-mounted voltage taps that streamline and simplify system implementations.

All six Riedon™ industrial shunt resistor by Bourns model types are available now, and are RoHS* compliant. For additional information, please see: www.bourns.com/products/resistors/current-sense-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

In April 2023, BE Services Company, Inc., a subsidiary of Bourns, Inc., purchased certain assets of Riedon, Inc., including its logo and trademarks and the right to continue to manufacture former Riedon™ products. “Riedon Logo” is a registered trademark of BE Services Company, Inc. in the United States. “Riedon” is a trademark of BE Services Company, Inc.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com