Search
Languages

Press Releases

2020

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.

2019

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.

2018

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.

2017

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.

2016

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.

2015

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.


2014

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.


2013

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.


2012

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.


2011

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.


201​0

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.


20​09

Bourns Introduces Automotive-Grade ChipGuard® Varistor Series that Delivers High Reliability, Fast-Response ESD Protection

Riverside, Calif., August 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its ChipGuard® Automotive MLA Series Varistor ESD Clamp Protectors Model specifically developed to protect sensitive automotive electronics from the threat of ESD up to IEC 61000-4-2 Level 4. Bourns' Model CGA-MLA Series are very fast bidirectional devices that deliver robust overvoltage protection and stable low leakage performance over a wide temperature range. The latest ChipGuard® devices from Bourns also feature multilayered varistor technology, and their proprietary insulating overcoat provides low and stable leakage current, quick response time (<0.5 ns) and high transient current capability. These features and benefits make the new varistor clamp protectors particularly well-suited to meet the ESD protection needs of HDMI, CANbus, Ethernet, sensor and touchscreen interfaces as well as GPS and camera links and other circuits sensitive to ESD.