Search
Languages

Bourns Releases Current Sensor Series that Features High Accuracy with Superior Operational Stability

The Riedon™ Model SSA-2 Analog Current Sensor by Bourns provides immunity to stray magnetic fields and meets unipolar power supply requirements

RIVERSIDE, Calif., December 2, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released its Riedon™ Model SSA-2 Series Analog Current Sensor by Bourns. These current sensors deliver a high accuracy current sensing solution with greater operational stability compared to typical Hall effect sensors. This series is designed to provide immunity to stray magnetic fields as they can detrimentally interfere with the operation of sensors in sensitive electronic devices, potentially causing inaccurate readings, device failure or even safety hazards. In addition, the Model SSA-2 Series meets unipolar power supply requirements, making these devices superior measurement choices for a wide variety of battery-related current sensing applications including large-scale energy storage banks, renewable energy generation infrastructure, industrial motor drives, building automation systems, and fuel cells.

The Model SSA-2 Series includes innovatively designed analog technology that could offer higher performance than Hall Effect technology, with ±0.1 % sensing accuracy and ±0.1 % linearity over their entire current range, with low susceptibility to temperature drift. In addition, the sensors’ low-noise resolution and offset performance allows accurate low-current measurements, and also provides excellent gain and linearity performance over the entire temperature range. Offering wide bandwidth AC and DC support, this series features nominal current range values from 100 A to 1000 A, making it more adaptable to different environments and a wide variety of market applications.

The Riedon™ Model SSA-2 Series Analog Current Sensor by Bourns is available now, and is RoHS* compliant. For additional information, please see: bourns.com/products/sensors/current-sensors.

About Bourns

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com