Search
Languages

Bourns' New Miniature Thermal Cutoff (TCO) Devices Provide High Current Capacity in Lighter, Smaller, More Robust Package

RIVERSIDE, Calif., February 27, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new series miniature Thermal Cutoff (TCO) devices that are lighter, smaller and offer high current capacity up to 13 A at 25 °C. Bourns designed its new TCO family to match the small space and overtemperature protection needs in next-generation Lithium-ion (Li-Ion) battery cells and USB 3.1 Type C cables.

Bourns' latest SC series and its previous-generation SA series devices are the only non-polymeric surface-mount TCO products available today. Surface-mount packaging provides significant benefits enabling manufacturers to board-mount them onto battery charge circuit boards, which can help to reduce assembly costs and supply chain lead times. The new SC series is 38 percent smaller than SA series yet has the same high current handling capacity. Its small size enables the SC series to be used in a wider range of battery-based applications where space and connector density require reliable, efficient overtemperature protection.

The SC series is available in two options: the SCxxAAA and SCxxAAB. The SCxxAAA features a reinforced cover that offers greater resistance to injection molding forces applied during USB cable manufacturing. The SCxxAAB series is thinner at just 0.94 mm, making it ideal for smartphone applications. Bourns SC Series TCO devices as well as the company's entire line of overtemperature battery protection solutions will be highlighted at Battery Japan, February 27 to March 1, 2019 in booth # W4-68.

Bourns SC Series TCO devices are available now, and are RoHS compliant* and halogen free**. For more detailed product information, please go to: www.bourns.com/products/circuit-protection/mini-breakers/product/SC.

* RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be “halogen free” if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk)†, audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com