Search
Languages

Bourns' New High Power TVS Diodes Deliver Industry-Standard Bidirectional Port Protection for AC/DC Power Line Applications

Riverside, Calif., March 4, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of new high Power TVS diodes that feature high current bidirectional port protection and meet industry standards including IEC 61000-4-5 8/20 µs current surge requirements. Designated Bourns® Models PTVS10-058C-TH and PTVS10-076C-TH, this new series of high power TVS diodes provides very high surge current protection with a peak pulse current rating of 10 kA and feature 58 V and 76 V standoff voltages, respectively. Designed using advanced silicon technology, Bourns' new models deliver lower clamping voltage under surge compared to Metal Oxide Varistor (MOV) technology.

"Bourns® Power TVS diodes are increasingly requested by customers that require robust circuit protection against power line surges and indirect lightning strikes in DC power bus clamping applications," said Ben Huang, Semiconductor Product Line Manager at Bourns, Inc. "These two new models offer lower clamping voltage under surge to provide a highly reliable solution that meets the protection and industry standards requirements of high power applications."

Pricing and Availability
As a pricing reference, the Bourns® Models PTVS10-058C-TH and PTVS10-076C-TH TVS Diodes are priced at $18.92 each in 10 piece quantities and $15.33 each in 500 piece quantities, respectively. Both models are available now in through-hole packaging and meet industry standards for Pb free solder reflow profiles for lead free packaging and are RoHS* compliant. For additional product specifications, please go to: www.bourns.com/docs/product-datasheets/PTVS10-TH.pdf.

About Bourns

Bourns is a privately held manufacturer of power electronics, resistive components, circuit protection, and sensing solutions. Founded in 1947 and headquartered in Riverside, California, Bourns serves the automotive, industrial, consumer, communications, healthcare†, and audio markets through a global network of design, manufacturing, and sales operations. For more information, visit bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com