Search
Languages

Bourns Introduces Air Coil Inductor Series with High Q, High Self-Resonant Frequency and Low Inductance Values

Offering lower losses and optimized for high frequency functionality, these new inductors give RF application designers a wider range of high Q solutions

RIVERSIDE, Calif., November 9, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced an air coil inductor series that features high Q, high self-resonant frequency and tight inductance tolerance. The Bourns® Model AC4842R Air Coil Inductor Series offers a high frequency, low loss solution that gives RF application designers a wider range of high Q solution options. Delivering a high Q value of at least 100 with inductance from 22 to 150 nanohenry (nH), these new air coil inductors are well-suited for today's high-frequency TV and radio receivers, radio transmitters and RF amplifier and tuning applications.

The series' features a wire coil design without a magnetic core, which provides significantly lower inductance values and offers superior functionality at high frequencies. Bourns designed the Model AC4842R Series with tight tolerance providing DC resistance from 4 to 33 milliohms, with 1.2 to 3.50 A maximum rated current and offering an operating temperature range from –25 to +125 °C. The Model AC4842R Series is also manufactured with an epoxy cover for added mechanical stability, and the series' surface mount design makes these air coil inductors ideal for pick and place processes.

The Bourns® Model AC4842R Series is available now, and is RoHS compliant*. For more detailed product information, please see: www.bourns.com/products/magnetic-products/air-coil-inductors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

 

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com