Search
Languages
Home / News / Press Releases / Press Release

Bourns Introduces Two New Series of Ceramic Core Constructed Wirewound Fixed Resistors

RIVERSIDE, Calif., May 19, 2015 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced two new series of low thermal resistant ceramic core wirewound resistors. These axial lead resistor families give designers an effective circuit conditioning solution for applications that have very high temperature and voltage requirements and operate in harsh environmental conditions. The Bourns® Model W and WS Series fixed resistors offer E24 resistance values, have been designed to operate at extreme temperatures from -55 °C to +200 °C and are coated in a material that meets the UL 94V-0 standard. Bourns introduced its latest wirewound fixed resistor series to meet the circuit conditioning needs of a broad range of industrial and consumer applications such as smart meters, white goods, power supplies, instruments/gauges, lighting and renewable energy systems.

The Bourns® Model W Series features a wide power range from 1 W to 10 W and provides resistance values ranging from 15 ohms to 150 ohms. It has been designed to withstand the surge from the 1.2/50 µs voltage waveform described in IEC 61000-4-5. The Bourns® Model WS Series has a power range of 1 W to 8 W and a resistance range of 15 ohms to 3.3K ohms.

"We specifically introduced the additions to our circuit conditioning product portfolio so our consumer and industrial electronic customers can meet ongoing application requirements for high temperature stability, enhanced power handling capabilities along with low resistance values," said Brian Ahearne, product line manager at Bourns, Inc. "These new families also complement the other circuit conditioning components offered by Bourns that include PTC resettable fuses, power inductors, rectifier diodes and Zener diodes."

Pricing and Availability
The Bourns® Model W and WS series wirewound fixed resistors are RoHS compliant* and available now. As a pricing reference, the Bourns® Model W3M is priced at $ 0.12 each in 10k piece quantities and Model WS3M is priced at $ 0.15 each in 10k piece quantities. For more information, please see the Bourns® Wirewound Fixed Resistor product page.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com