Search
Languages

Bourns Introduces its Smallest Miniature Resettable Thermal Cutoff (TCO) Devices

RIVERSIDE, Calif., October 16, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced the company's smallest miniature resettable Thermal Cutoff (TCO) devices designed for overtemperature and overcurrent protection of lithium polymer and prismatic cells. The Bourns® Model CB Series is the company's next generation of axial leaded TCO devices that control abnormal, excessive current virtually instantaneously, up to rated limits. This latest series is more than 26 percent smaller than Bourns' successful NR Series, yet has the same current carrying capability. The devices' low-profile 0.8 mm height and body width of 2.5 mm makes this series ideal for smaller batteries in smartphones and portable electronics, yet their high current carrying capability also makes them optimal for next-generation notebook and tablet PC battery cells.

Offering resistance levels as low as 2.2 milliohms, the Bourns® Model CB Series has current capabilities from 6 A up to 11 A at 60 °C as well as a welding projection option. These new miniature resettable TCO devices are available in four trip temperature options of 72 °C, 77 °C, 82 °C and 85 °C with a ±5 °C tolerance. The temperature options can be further narrowed upon request. In addition, the construction of the CB Series uses a high corrosion resistant bimetal mechanism to withstand most humid environments.

Available now, Bourns® Model CB devices are RoHS compliant* and halogen free** with UL agency recognition. For more detailed product information, please see www.bourns.com/products/mini-breakers/product/CB.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

***Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com