Search
Languages

Bourns Announces Versatile Square-Package Air Coil Inductor Series Featuring a High Q Value and High Self-Resonant Frequency

New air coil inductors meet today’s high-frequency application demands for enhanced signal filtering, efficient energy transfer and tight inductance tolerance

RIVERSIDE, Calif., January 29, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its AC3028SQ, AC5037SQ, ACXX14SQ, ACXX15SQ, and ACXX18SQ Series Air Coil Inductors. The five new series deliver High Q and high self-resonant frequency (SRF) with tight inductance tolerance that enables designers to meet ongoing demands for smaller, faster and more compact electronics. These new air coil inductors feature a square package design with a flat top and bottom that streamlines reliable pick-and-place assembly while providing superior mechanical stability.

Other significant features of the five new inductor series include high Q values up to 230, with inductance ranging from 5.5 to 82 nanohenries (nH), making them ideal for today’s high-frequency TV and radio receivers, radio transmitters, RF amplifiers and tuning application designs. In addition, Bourns® AC3028SQ, AC5037SQ, ACXX14SQ, ACXX15SQ, and ACXX18SQ Series Inductors have a tight tolerance of 2 percent and 5 percent, with DCR values that range from 3.4 to 12 milliohms (mΩ). These air coil inductors offer rated current values from 2.7 to 5.6 A and feature an operating temperature range of from -25 °C to +125 °C.

Bourns® AC3028SQ, AC5037SQ, ACXX14SQ, ACXX15SQ, and ACXX18SQ Series Air Coil Inductors are available now and are RoHS compliant*. For more detailed product information, please see: bourns.com/products/magnetic-products/air-coil-inductors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf