Search
Languages

Bourns Adds Four New Model Families to its Environmental Pressure Sensor Line

RIVERSIDE, Calif., February 26, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the addition of four new model families to the Bourns® Precision Sensor (BPS) line. Based on state-of-the-art Micro-Electro-Mechanical Systems (MEMS) technology, the four new BPS310, BPS320, BPS330 and BPS340 series are cost-effective pressure sensor solutions that feature ultra-fast response times, high resolution, and long-term stability. These features, along with the ability to work with pressure ranges from 5 to 500 psi, make Bourns' latest BPS sensors ideal for a vast array of packaging requirements and applications including industrial systems and low/medium risk medical† devices.

The Model BPS310 series is designed to provide high sensitivity/accuracy for ultra-low pressures. For gauge and pressure measurement, the Model BPS320 series offers a robust configuration in a surface mount package. The Model BPS330 series is a through-hole pressure sensor with an aluminum port for low pressure applications with an operating range up to 125 °C. With an ability to handle certain harsh medias, the Model BPS340 series is offered in a surface mount package capable of supporting pressure ranges up to 500 psi.

Bourns® BPS310, BPS320, BPS330 and BPS340 series sensors are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/sensors/environmental-sensors

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

About Bourns

Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical (low/medium risk), audio and various other market segments. Additional company and product information is available at www.bourns.com.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

Agency Contact:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Company Contact:
David Scofield
Bourns, Inc.
(951) 781-5054
david.scofield@bourns.com