Search
Languages

Bourns to Present Inductive Steering Sensor Technologies at ATC Shanghai 2026

RIVERSIDE, Calif., May 26, 2026 - As electric power steering systems and steer-by-wire architectures place tighter demands on position and torque measurement, Bourns will exhibit its inductive sensing solutions for automotive steering applications at the 2026 ATC Shanghai International Automotive Chassis System Technology Exhibition, June 3–5, at the Shanghai New International Expo Centre. The company will exhibit at Booth #E56049.

Bourns’ steering sensor portfolio includes torque angle sensors (TAS), steering angle sensors (SAS), and linear position sensors (LPS). These products target applications in electric power steering and chassis systems where ADAS integration requires precise, fault-tolerant position data across the operating temperature range. Bourns automotive grade components are manufactured in IATF 16949-certified facilities, and are compliant to applicable AEC-Q standards, and supported by PPAP Level 3 documentation.

The portfolio uses a platform-based hardware architecture, allowing OEMs and Tier 1 suppliers to apply common mechanical and electrical interfaces across multiple vehicle programs.

Technical Forum Presentation

Felix Merkle, Product Line Manager for Bourns Steering Sensors, will present at the ATC Shanghai Technical Forum from 14:20 to 14:45 on June 3. His session will examine inductive sensing as an alternative to resolver-based and Hall-effect approaches in modern steering systems—covering measurement principle, interference immunity, functional safety considerations, and architectural fit for current EPS and emerging steer-by-wire designs.

 

“Steering systems in electrified and ADAS-equipped vehicles require position and torque measurement that remains accurate under high electromagnetic load and across a wide thermal range,” said Merkle. “Inductive sensing addresses those constraints in ways that magnetic sensors handle less cleanly, and we’ll walk through the tradeoffs at the forum.”

Bourns engineers will be available at Booth #E56049 throughout the exhibition to review application requirements and discuss interface specifications with OEMs and Tier 1 engineers.

Event Details
  • Event: ATC Shanghai 2026 International Automotive Chassis System Technology Exhibition
  • Dates: June 3–5, 2026
  • Venue: Shanghai New International Expo Centre, Shanghai, China
  • Booth: #E56049

Media Contact
Josephine Chen

Bourns Asia Pacific, Inc.
TEL: (886) 2-2562-4117 ext. 138
Email: Josephine.chen@bourns.com

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com