Search
Languages

Bourns、業界をリードするギター用ポテンショメーター製品に新オプションを発表

Riverside, Calif., January 10, 2012 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that it has released a series of new product options to its industry-leading line of guitar potentiometers. Bourns has developed a specialty line of potentiometers for electric and bass guitars to upgrade these instruments for improved sound quality, reliability and longevity. The following five new model options will be showcased in Bourns' booth #5696 at the upcoming NAMM Show, January 19-22, 2012 in Anaheim, California. The "no load" guitar potentiometer is designed with a long-wearing insulator and a positive action detent for improved reliability. The left-handed potentiometers have special reverse audio tapers and a logarithmic curve specifically designed for excellent volume response at all positions along the potentiometer. The long bushing potentiometers are excellent for use in solid body guitars and work in all types of electric or bass guitars, with or without a push-pull switch.

"Bourns continues to introduce new product options that help our customers get the highest quality out of their guitars and associated professional audio equipment," said Chuck Manzano, product manager at Bourns, Inc. "We have an ongoing commitment to meet market needs. After listening to our customers, these new options for electric and bass guitars that are being released at NAMM are in direct response to customer requests for higher quality alternatives to some commonly used products." with or without a push-pull switch.

As a pricing reference, Model PDB241-GNL is priced at $2.25, Model PDB241-GTR is priced at $1.75, Models PDB181-GTR (left handed and long bushing) are priced at $0.95 and $1.25 respectively and Model PDB183-GTR is priced at $3.85. All prices are based on quantities of 1,000. All models are available through Bourns authorized distributors and Pro Audio resellers.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf