MENU
Search
Languages

Bourns Announces Revolutionary New Hot Dipped Tin Plating Process That Prevents Tin Whiskers

Riverside, Calif., February 10, 2009 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company is implementing the use of a revolutionary hot dipped tin plating process on its entire line of RoHS-compliant cermet wire terminal trimming potentiometers. A recommended technology by iNEMI, hot dipped tin plating is a proven tin whisker inhibiting process. This new plating process is environmentally-friendly, while providing a high level of reliability and product durability. The new hot dipped tin plating process also alleviates concerns OEMs may have with RoHS compliancy or the arduous process for certification. Bourns sought a new plating process from the industry-standard matte tin plating to improve quality, value and durability of its products to meet customer requirements. Bourns’ industry-leading trimming potentiometers are designed into a broad range of applications and industries that include consumer electronics, telecommunications, military, aerospace and medical.

Tin whiskers are electrically conductive, crystalline structures of tin that can grow from surfaces where tin is used as a final finish and can cause short circuits, interference and unreliability. Tin whiskers have been a concern since RoHS legislation mandated the removal of lead from the terminal plating of all electronic components. Bourns has been manufacturing RoHS-compliant trimming potentiometers with matte tin plating since the legislation became law. Based on new industry requirements and recommendations, Bourns implemented the new hot dipped tin plating process. Bourns will continue to offer non-RoHS compliant tin/lead plated products as customer demand warrants.

“Numerous electronic system failures have been attributed to short circuits caused by tin whiskers,” said Emill Melliz, potentiometer product line manager at Bourns. “We are confident that the breakthrough hot dipped tin plating process will become the industry-standard replacement for tin/lead plating. Demonstrating Bourns leading position in manufacturing highly reliable trimming potentiometers, this change in the plating process reflects the value we place on quality and exceeding the needs of our customers.”

Availability
Bourns’ entire RoHS-compliant line of trimming potentiometer products with hot dipped tin plating is available now. For complete model numbers and sizes, go to Bourns’ website at https://www.bourns.com/en/products/resistive-products.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf