Search
Languages

Bourns® CRN Series Thick Film Resistors Deliver Precise, Reliable Low-ohmic Current Sensing in Compact Package

Constructed with cost-effective metal thick film technology, new resistors offer power ratings up to 2W to support high-density, space-constrained power circuit designs

RIVERSIDE, Calif., November 25, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its Bourns® CRN Series Thick Film Resistors. Designed to deliver precise, reliable low-ohmic current sensing in a compact package, the CRN Series offers high power ratings up to 2 W to support today’s high-density power circuit designs. Constructed using a more cost-effective and lead-free metal thick-film paste instead of carbon, the CRN Series achieves RoHS* compliance without exemption, minimizing customer concerns over restricted substances.

These new resistors are available in a range of compact package sizes (from 0603 to 2512) and designers can select resistance values from 47 milliohms (mΩ) to 10 ohms (Ω). In addition, the series supports an operating temperature range of –55 °C to +155 °C, and has been qualified against IEC 60115-1 test requirements for overload, operational life, solder heat, solderability, and board flex. With its balance of low resistance values, high power density and environmental compliance, the CRN Series offers a robust, economical current sensing solution for a broad variety of electronic designs that include battery charge management, Battery Management Systems (BMS), low-voltage power supplies, industrial controllers, digital meters and current measurement applications.

Bourns® CRN Series Thick Film Resistors are available now through Bourns’ authorized distribution partners and are RoHS* compliant and lead-free. For more detailed product information, please see: bourns.com/products/resistors/thick-film-chip-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf