Search
Languages

Bourns® CRN Series Thick Film Resistors Deliver Precise, Reliable Low-ohmic Current Sensing in Compact Package

Constructed with cost-effective metal thick film technology, new resistors offer power ratings up to 2W to support high-density, space-constrained power circuit designs

RIVERSIDE, Calif., November 25, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its Bourns® CRN Series Thick Film Resistors. Designed to deliver precise, reliable low-ohmic current sensing in a compact package, the CRN Series offers high power ratings up to 2 W to support today’s high-density power circuit designs. Constructed using a more cost-effective and lead-free metal thick-film paste instead of carbon, the CRN Series achieves RoHS* compliance without exemption, minimizing customer concerns over restricted substances.

These new resistors are available in a range of compact package sizes (from 0603 to 2512) and designers can select resistance values from 47 milliohms (mΩ) to 10 ohms (Ω). In addition, the series supports an operating temperature range of –55 °C to +155 °C, and has been qualified against IEC 60115-1 test requirements for overload, operational life, solder heat, solderability, and board flex. With its balance of low resistance values, high power density and environmental compliance, the CRN Series offers a robust, economical current sensing solution for a broad variety of electronic designs that include battery charge management, Battery Management Systems (BMS), low-voltage power supplies, industrial controllers, digital meters and current measurement applications.

Bourns® CRN Series Thick Film Resistors are available now through Bourns’ authorized distribution partners and are RoHS* compliant and lead-free. For more detailed product information, please see: bourns.com/products/resistors/thick-film-chip-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com