Search
Languages

Offering ESD Protection Flexibility, Bourns Unveils TVS Diode Series Available in Space-Saving DO-214AB Package

New series with 21 unidirectional and bi-directional models features broad working peak reverse voltage range from 12 V to 30 V

RIVERSIDE, Calif., November 19, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today unveiled its 5.0SMDJ Series Transient Voltage Suppressor (TVS) Diodes. Available in a space-saving, compact DO-214AB package, the new series is designed to provide effective Electrostatic Discharge (ESD) protection for portable communications, computing and video equipment applications. The Bourns® 5.0SMDJ Series includes 13 unidirectional models and eight bi-directional models.

Offering high performance energy absorption and clamping capabilities, these new TVS diodes enable designers to select from a broad working peak reverse voltage range from 12 V to 30 V. The 5.0SMDJ Series also features peak pulse power of 5,000 watts and breakdown voltage up to 36.8 V with typical fast response times of less than 1 nanosecond to clamping after breakdown initiation. The series has also been tested to JEDEC standards.

The Bourns® 5.0SMDJ Series TVS Diode is available now through Bourns’ authorized distribution partners and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/diodes/tvs-diodes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf