Search
Languages

Bourns Announces Two Automotive Grade Semi-shielded Power Inductor Series Engineered for High Reliability

Featuring bottom-soldered lead wire construction, the new series provides enhanced mechanical strength and stability making them ideal for mission-critical applications

RIVERSIDE, Calif., June 28, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced two new AEC-Q200 compliant, automotive grade semi-shielded power inductor series whose bottom-soldered lead wire construction offers enhanced mechanical strength and stability. Bourns designed the new Model SRN4012BTA and SRN4018BTA series as a high-reliability solution for mission-critical applications such as automotive systems, power supplies, DC-DC converters, and in various industrial and telecom electronics.

The Bourns semi-shielded structure combines the features of non-shielded and shielded inductors, providing lower magnetic field radiation than non-shielded inductors and a more cost-effective alternative to fully shielded ferrite-based inductors. These new ferrite core, enameled copper wire power inductors offer inductance values from 0.47 to 100 µH and an operating temperature range of –55 °C to +125 °C.

Bourns® Model SRN4012BTA and SRN4018BTA semi-shielded power inductor series are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf