MENU
Search
Languages

美国柏恩(Bourns)推出增强温度性能的大功率电压瞬变抑制二极管

河边市, 加州, Feb 26, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced new high power TVS diodes for use in DC bus protection applications. The new models deliver high current bidirectional port protection that meets IEC 61000-4-5 8/20 µs current surge requirements and are RoHS* compliant. Designated Bourns® Models PTVS6-058C-TH and PTVS6-076C-TH, this new series of power TVS diodes provide enhanced temperature performance for greater system stability and increased reliability. Designed using advanced silicon technology, Bourns' new devices offer lower clamping voltage under surge compared to Metal Oxide Varistor (MOV) technology. In Bourns' testing, the new models have exhibited an excellent surge response versus temperature; the typical maximum surge current at 150 °C 75 % of their rated value at 25 °C.

"We designed Bourns' two new high power TVS diodes with enhanced temperature performance to meet robust circuit protection requirements that offer superior protection against power line surges and indirect lightning strikes in AC and DC power line applications," said Ben Huang, Semiconductor Product Line Manager at Bourns, Inc. "Our new diode series also provides excellent surge performance and temperature ratio benefits that are critical requirements in today's demanding high power applications."

Both Bourns® models provide very high surge current protection with a peak pulse current rating of 6 kA. The Bourns® Model PTVS6-058C-TH features a 58 V standoff voltage and the Bourns® model PTVS6-076C-TH has a 76 V standoff voltage.

Pricing and Availability
As a pricing reference, the Bourns® models PTVS6-058C-TH and PTVS6-076C-TH are priced at $13.78 each in 10 piece quantities and $12.60 each in 500 piece quantities, respectively. Both models are available now. For additional product specifications, please go to: www.bourns.com/docs/product-datasheets/PTVS6-TH.pdf.

关于美国柏恩(Bourns)

Bourns — 是电子零组件业界的龙头制造供货商,公司总部位于美国加州的河边市,其产品包含:位置与速度传感器、电路保护解决方案、磁性组件、微电子模块、面板控制器及电阻产品,服务产业涵盖汽车、工业、消费、通信、非关键性的生命支持医疗(低/中风险)、音频以及其他各种市场。如需了解更多的公司与产品讯息,欢迎上公司网站查询:www.bourns.com