MENU
Search
Languages

美国柏恩(Bourns)推出AC/DC电源线应用的大功率瞬态电压抑制器新型号

河边市, 加州, Jan 28, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of new high Power TVS diode models in SMD packaging for use in AC and DC power line applications. The new models feature high current bidirectional port protection meeting IEC 61000-4-5 8/20 µs current surge requirements and are RoHS* compliant. Designated Bourns® Models PTVS15-058C-SH and PTVS15-076C-SH, these Power TVS diodes offer enhanced performance stability and increased reliability. Designed using advanced silicon technology Bourns' new devices deliver lower clamping voltage under surge compared to Metal Oxide Varistor (MOV) technology. The SMD package provides a 20% reduction in peak clamping voltage compared to an equivalent through-hole device because of its lower lead inductance. The result is reduced electrical stress on the protected circuitry. Additionally, the SMD package simplifies assembly and can reduce costs by eliminating the extra design requirements in cases where the Power TVS diode is the only through-hole component on the printed circuit board.

"Bourns' Power TVS diodes are becoming increasingly popular because they provide robust circuit protection against power line surges and indirect lightning strikes in AC and DC power supplies used in telecom and other exposed applications," said Ben Huang, Semiconductor Product Line Manager at Bourns, Inc. "We designed these new models with specific packaging technology giving our customers the benefit of a highly reliable solution that meets the growing protection demands of today's high power applications."

Bourns' new Power TVS diode models also exhibit an excellent surge response versus temperature, with a maximum surge current rating at 150 °C, which is 70% of their rated value at 25 °C. Both models provide very high surge current protection with a peak pulse current rating of 15 kA. The Bourns® Model PTVS15-058C-SH features a 58 V standoff voltage and the Bourns® model PTVS15-076C-SH has a 76 V standoff voltage.

Pricing and Availability
As a pricing reference, the Bourns® models PTVS15-058C-SH and PTVS15-076C-SH are priced at $19.70 each in 10 piece quantities and $17.50 each in 500 piece quantities respectively. Both models are available now. For additional product specifications, please go to: www.bourns.com/docs/product-datasheets/PTVS15-SH.pdf.

关于美国柏恩(Bourns)

Bourns — 是电子零组件业界的龙头制造供货商,公司总部位于美国加州的河边市,其产品包含:位置与速度传感器、电路保护解决方案、磁性组件、微电子模块、面板控制器及电阻产品,服务产业涵盖汽车、工业、消费、通信、非关键性的生命支持医疗(低/中风险)、音频以及其他各种市场。如需了解更多的公司与产品讯息,欢迎上公司网站查询:www.bourns.com