Search
Languages

Bourns Announces Extension to its Incremental Encoder Product Line Offering a 25 mm Shaft Length Option

Additional shaft length options to Bourns® PEC11S Series encoders give designers a more robust solution that helps maintain stability and resists environmental stresses

RIVERSIDE, Calif., July 11, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced an extension to its PEC11S Series incremental encoder product line to now offer a 25 mm shaft length option. In addition, designers now can order Bourns® PEC11S encoders with a 25 mm flat-type shaft length option. The availability of these shaft selections gives designers enhanced load-bearing support for better application stability or to withstand environmental stresses.

The advanced features designed into the PEC11S Series remain available, including its IP40 rating, 15,000 rotational cycle life and the -40 °C to +70 °C operating temperature range. The additional and existing features and options available with Bourns® PEC11S encoders make them particularly beneficial as motion measurement solutions for applications such as audio-visual equipment, consumer electronic appliances, radios, musical instruments and communications equipment.

The extension to the Bourns® Model PEC11S Series incremental encoders is available now and is RoHS compliant*. For more detailed product information, please see: bourns.com/products/encoders/contacting-encoders.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf