Search
Languages

Bourns Releases PDB241-GTR Series Guitar Potentiometer Product Extension

New product extension significantly increases the rotational life to 100,000 cycles to meet higher durability demands from frequent users

RIVERSIDE, Calif., May 12, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that the Company has released a product extension of its popular PDB241-GTR Series guitar potentiometers. This extension significantly increases the rotational life to 100,000 cycles, supporting the high-use demands of dedicated performers. With this extension, Bourns is also making a standard option available that offers a rotational life of 15,000 cycles.

In addition to the PDB241-GTR Series 100,000-cycle rotational life, it features low torque of 10 to 45 g-cm, a -10°C to +70°C operating temperature range as well as metal knurled and metal plain shaft options. These capabilities help ensure that when the guitar potentiometer is used in an instrument, the player gets the advantage of using a smooth-working component that more easily allows them to achieve the sound/effect they are trying to create on their guitar. This guitar potentiometer product extension is specifically suited for electric and bass guitars with thick bodies, and is engineered to meet players’ enhanced quality, reliability and durability expectations.

The Bourns® PDB241-GTR Series product extension is available now and is RoHS* compliant. For more detailed product information, please see: bourns.com/products/potentiometers/commercial-panel-controls.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf