MENU
Search
Languages

Bourns Announces Air Coil Inductor Series with a High Q Value and High Self-Resonant Frequency

New air coil inductors meet today’s high frequency application demands for enhanced signal filtering, efficient energy transfer and tight inductance tolerance

RIVERSIDE, Calif., April 8, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new air coil inductor series that features a high Q value and high self-resonant frequency. Designed as a low energy loss solution for today’s high frequency applications, Bourns® AC1060R, AC2213R, AC3630R, AC4013R and AC6830R Series Air Coil Inductors offer significantly lower inductance values, tight inductance tolerance and operate at higher frequencies.

These new air coil inductors are wire-coil (without magnetic core) constructed, which contributes to substantially lower inductance values for excellent functionality at high frequencies. With high Q values from 87 to 145 and inductances from 1.65 to 538 nanohenries (nH), Bourns® Air Coil Inductors are ideal for a broad range of next-generation TV and radio receivers, radio transmitters and RF amplifier and tuning applications. The series’ tight tolerance provides DC resistance from 1.1 to 90 milliohms, up to 4 A maximum rated current and has an operating temperature range from -25 to +125 °C. The air coil inductors also feature an epoxy cover for mechanical stability and to help support pick and place manufacturing automation processes.

The Bourns® AC1060R, AC2213R, AC3630R, AC4013R and AC6830R Series Air Coil Inductors are available now and are RoHS* compliant. For more detailed product information, please see: bourns.com/products/magnetic-products/air-coil-inductors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf