Search
Languages

Bourns Announces Two Thick Film Resistor Series that Deliver High Power Dissipation in Compact TO-220 and DPAK Packaging

Riedon™ Model PF2203/PFS35 Series High Power Thick Film Resistors by Bourns dissipate up to 35 W of power with low TCR and tolerance options

RIVERSIDE, Calif., November 18, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its Riedon™ Model PF2203 and PFS35 Series High Power Thick Film Resistors by Bourns. Adding to Bourns’ broad high-power resistor line, the two series are available in compact TO-220 and DPAK packages, offering low inductance, excellent pulse handling capabilities, and elevated power ratings of 35 W that enable enhanced circuit stability and measurement accuracy.

The Riedon™ Model PF2203 and PFS35 Series High Power Thick Film Resistors by Bourns feature a wide resistance value range from 10 Megohms to 51 Kiloohms, have a temperature range of -55 to +175 °C and are available with resistance tolerance options of ±1 percent and ±5 percent. Bourns is offering these resistors to match market demands for greater power dissipation in smaller packages. Surface mount packaging, such as the DPAK offered with the Model PFS35 Series, is also particularly popular for its ability to help reduce manufacturing costs.

The features of these thick film resistors make them ideal solutions to meet current limiting, current measurement, and capacitor discharge requirements in a broad variety of applications, including industrial motor drives, AC-DC and DC-DC power converters, and Battery Energy Storage Systems (BESS).

The Riedon™ Model PF2203 and PFS35 Series High Power Thick Film Resistors by Bourns are available now, and are RoHS* compliant. For additional information, please see: www.bourns.com/products/resistors/high-power-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf