Search
Languages

Bourns Unveils Shielded Power Inductor Series Designed with a Ferrite Core and Ferrite Shield for Low Magnetic Field Radiation

New AEC-Q200 Compliant, Automotive Grade inductors are ideal for applications that operate in low noise environments or those that require higher inductor reliability

RIVERSIDE, Calif., February 20, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its new Model SRR5228A and SRR5828A Series Shielded Power Inductors. These are Bourns® latest AEC-Q200 compliant, automotive grade power inductors and are designed with a ferrite core and ferrite shield. This construction delivers low magnetic field radiation, which is essential for applications that operate in low noise environments such as in automotive driver assistant devices, infotainment systems and lighting designs. These inductors are also well-suited for DC-DC converters and power supplies in consumer, industrial and telecom applications where higher inductor reliability is a frequent requirement.

Providing industry-leading inductance and heating current, the Model SRR5228A and SRR5828A Series feature an inductance range up to 1000 μH and heating current up to 5.2 A. These inductors also offer a broad operating temperature range of -40 °C to +150 °C.

Bourns® Model SRR5228A and SRR5828A Shielded Power Inductor Series are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf