Search
Languages

Bourns Unveils Bourns' Highest Current Carrying PTVS Diode Series in a Compact DFN Package

New bidirectional PTVS diode family features 20 kA, 8/20 µs surge handling capability with low clamping voltage designed for high power DC line applications

RIVERSIDE, Calif., January 4, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released Bourns' highest current carrying bidirectional Power Transient Voltage Suppressor (PTVS) Diode series that is available in a compact surface mount DFN package. Bourns® Model PTVS20-015C-H is capable of handling 20 kA, 8/20 µs current surge at a low voltage of 15 V. These features deliver effective electrostatic discharge (ESD) protection in applications that require high power DC line protection.

The Bourns® Model PTVS20-015C-H PTVS Diode meets IEC 61000-4-2 Level 4 ESD protection requirements. It also features low clamping voltage at peak pulse current and assists in meeting IEC 61000-4-5 8/20 μs current surge requirements for lightning protection.

In order to support large currents such as 60 kA in next-generation applications, designers typically have had to connect many devices with low current handling capability in parallel. With a single device capable of handling 20 kA, a fewer number of devices can now be connected in parallel to achieve the same desired protection level. This reduces the total BOM count and can help save valuable space on the PCB.

The Bourns® Model PTVS20-015C-H is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/diodes/power-tvs-diodes

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf