Search
Languages

Bourns Introduces Advanced Hybrid Position Sensor Designed for Certain Harsh Environment RS-485-based Applications

New Model HES38U-RS485 offers high quality, long life solution that features a 5 million shaft revolution rotational life and an IP65 rating

RIVERSIDE, Calif., April 28, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced an innovative hybrid position sensor for RS-485-based applications in certain harsh environments. Designed to meet the specifications of heavy-duty applications requiring long cycle life and high reliability, the new Bourns® Model HES38U-RS485 hybrid position sensor offers a rotational life of up to 5 million shaft revolutions with 10 turns of absolute position. It has an Independent Linearity specification of ±0.1 % max, an IP65 seal rating and an operating temperature range of -40 °C to +85 °C.

The advanced hybrid design enables the Model HES38U-RS485 to deliver enhanced linearity, resolution and accuracy. Highly repeatable and resistant to vibration/shock and fluid/dust ingress, this robust position sensor is an optimal solution for a variety of industrial feedback applications including patient platform positioning, 3D imaging position, pneumatic control valve position and actuator motor position as well as for automated manufacturing robotics.

It features a 6 mm diameter slotted shaft supported by a mechanical angle of 3600 ° ±10 ° and is available with customized longer cable lengths and in a servo mount configuration. The Bourns® Model HES38U-RS485 is available now and is RoHS* compliant. For more detailed product information, please see: www.bourns.com/products/sensors/position-sensors/non-contacting-multiturn

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf