Search
Languages

Packed with Additional Design Options, Bourns Announces Three New Rotary Potentiometer Model Series

Bourns® Potentiometers Offer Switch, Shaft Length and Vertical and Horizontal PC Pin Orientation Options with an IP 40 Seal Rating

RIVERSIDE, Calif., April 19, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced three new rotary potentiometer model series that provide enhanced features and multiple new design options. The Model PRS11R Rotary Metal Shaft Potentiometer series, Model PRS12R Rotary Metal Shaft Potentiometer series and Model PRS14R Rotary Plastic Shaft Potentiometer series give designers additional switch, shaft configuration, vertical and horizontal PC pin orientation and detent options depending on the model. The versatility provided by these options makes the new Bourns® rotary potentiometers ideal solutions for a wide variety of User Interface Controls in professional audio and lighting applications, low/medium risk medical* and laboratory equipment, and industrial automation controls.

All three-model series have an IP 40 seal rating and feature a small form factor with through-hole type mounting. The Model PRS11R has a 15,000 rotational cycle rating, a -20°C to +70°C operating temperature range and momentary switch and flatted shaft options. The Model PRS12R series features a 10,000 rotational cycle rating and is available with flatted, slotted and knurled shaft as well as detent options. The Model PRS14R series also has a 15,000 rotational cycle rating, with a -10°C to +70°C operating temperature range and a detent option.

Bourns® Model PRS11R, Model PRS12R and PRS14R rotary potentiometer series are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/potentiometers/commercial-panel-controls

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf