Search
Languages

Bourns Adds 3D, SPICE Model, S-Parameter and LTspice Design Files to Company Website

Riverside, Calif., December 4, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the addition of 3D, SPICE model, S-Parameter and LTspice files to the company’s website. Beneficial for circuit modeling and to simulate device performance, Bourns offers its 3D model files in IGS and STP formats, SPICE Model files in TXT or DOC formats, S-Parameter files in S2P formats, and LTspice files in LIB formats. Bourns has also made it easy for designers to find the new files by placing them in three locations on its homepage: on the "Data Sheet" search, from individual product pages and by clicking the "Design Files" button.

Bourns provides 3D model files on most of its product lines. SPICE model files are currently available for several Bourns® TBU® high-speed protectors (TXT), TVS diodes (DOC), and is offering S-Parameter (S2P) and LTspice (LIB) files for many of its inductor products. By supplying its SPICE files with the Bourns® component’s critical specifications, engineers can simply load them into the program, test their circuit and make an informed decision about the device in their application. Compared to taking this essential information from the data sheet, access to these new design tools allows engineers to speed prototyping and application development, thus saving consideration time and costs.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf