Search
Languages

Bourns Introduces Non-Contacting Rotary Position Sensor

Riverside, Calif., October 25, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new non-contacting magnetic rotary position sensor which can help increase product lifespan and reliability of applications that operate in harsh and high vibration environments. Designated Bourns® Model AMS22, the sensor utilizes magnetic hall-effect technology that enables high performance operation even in severe temperature or unclean conditions. The new sensor is the latest addition to the company's sensor product line, and is designed to meet OEM requirements for a cost-effective, long life position sensor that improves reliability. Bourns® non-contacting rotary position sensor is an ideal solution for value and actuator position feedback, camera and antenna location identification and precision positioning requirements in a wide range of applications that include medical diagnostic and general industrial equipment.

"The release of Bourns' new non-contacting rotary position sensor is in direct response to our customers' requirements for solutions that help extend product life and reliability in an increasing number of applications that must operate in extreme environmental conditions," said John Kelly, General Manager Industrial Market at Bourns, Inc. "Designed to maintain its magnetic orientation even during redundant mechanical operation, this new sensor provides an excellent solution to applications that are dormant for extended periods of time but require precise position information on demand. Bourns is committed to continued development of solutions that help our customers solve tough technology issues. We are not just delivering a new product, we are launching a new technology platform that will meet the existing and future needs of the Industrial, Consumer and Automotive markets we serve."

Bourns' non-contacting rotary position sensor helps improve product longevity up to fifty million cycles depending on the product and particular application. The new sensor has an analog single output from 0.1 to 4.9v, with an effective electrical output of 340 degrees and is programmable up to 360 degrees. The analog output features a 12 bit resolution and comes with independent linearity of 0.5% or 0.3%.

Pricing and Availability
The new non-contacting rotary position sensor is available now in production quantities. As a pricing reference, the Bourns® Model AMS22 is offered at $12.50 for 10,000 piece quantities through distribution.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf