MENU
Search
Languages

Bourns Releases Extended Range of Non-Isolated DC/DC Converters

Riverside, California, August 1, 2005 Bourns, Inc. is pleased to announce the release of an extended range of non-isolated dc/dc converters in industry-standard packaging.

Bourns® Switch Power™ Product Group has been providing cost-effective, quality power solutions since 1995. The company's non-isolated converters provide the low voltages needed to support core logic, ASICs, microcontrollers and microprocessors. These high-efficiency converters provide improved regulation and superior dynamic response.

Bourns® Switch Power™ Product Group recently added the X and XT series of low-cost non-isolated dc/dc converters, which utilize the latest buck topologies and synchronous rectification to achieve efficiencies up to 95%.

Nominal input voltages are 3.3 V, 5 V and 12 V, with output voltages of 0.75 V to 5.5 V dependent on input voltage. Output currents begin at 0 A, and have maximum outputs of 5 A, 6 A, 10 A, and 16 A for any combination of the input and output voltages described above.

The X and XT series converters are loaded with key features such as an adjustable output voltage (also available as fixed output voltage), remote sense capability, slow start, user on/off, an operating temperature range of -40¡ C to +85¡ C and sequencing (XT only). They are available in industry standard RoHS compliant SIP (single- in-line package) and compact SMD (surface mount device) configurations.

Pricing for quantities of 1,000 pieces is $4.75, $5.25, $8.75 and $10.50 for the 5 A, 6 A, 10 A and 16 A device respectively. Samples are available upon request.

For detailed electrical and mechanical specifications, please check the Bourns website, at www.bourns.com, under "DC/DC Converters". Design verification test reports are available from product management on request to assist with your design-in process.

Please contact Andrew Barrett for further information at andrew.barrett@bourns.com.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com