Search
Languages

Bourns Expands Industry-Leading Modular Contacts Portfolio with Five, Six and Eight Amp Products

Innovatively designed modular contacts meet higher power delivery demands for energy charging, efficient energy transfer or to support parallel loads and multiple subsystems

RIVERSIDE, Calif., March 18, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that it has expanded its modular contacts portfolio with new five, six and eight amp products. The unique, advanced design of Bourns® 75ABF, 75ABM, 76AAF, 76AAM, 78ADF and 78ADM Modular Contacts gives designers additional higher amperage and power-dense choices. They also are tested for 50,000-cycle operation and can be stacked side-by-side to enable greater design flexibility.

Designers can realize multiple benefits from employing these latest higher-amp modular contacts, including enhanced power delivery for demanding application tasks, the ability to quickly charge batteries and to provide the capability for efficient energy transfer that reduces voltage drop over short distances. In addition, Bourns® new five, six and eight amp Modular Contacts deliver the scalability to support multiple subsystems.

Bourns® 75ABF, 75ABM, 76AAF, 76AAM, 78ADF and 78ADM Modular Contacts are available now and are RoHS compliant*. For more detailed product information, please see: bourns.com/products/connectors/modular-contacts.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf