Search
Languages

Bourns Adds New Model to Company’s Line of AEC-Q200 Compliant, Automotive Grade Semi-shielded Power Inductors

New Model SRN3010BTA-330M features high inductance value to optimize circuit performance and bottom-soldered lead-wire that enhances reliability

RIVERSIDE, Calif., March 12, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that it has added a new high inductance model to its SRN3010BTA Series Semi-shielded Power Inductors. The new Model SRN3010BTA-330M features an inductance value of 33 microhenries (µH) for efficient current handling. Its bottom-soldered lead-wire offers increased mechanical strength and stability for enhanced product reliability.

This power inductor model’s 1 mm max. profile semi-shielded structure combines the features of non-shielded and shielded inductors, providing lower magnetic field radiation than non-shielded inductors, and is considered a more cost-effective alternative to fully-shielded ferrite-based inductors. Offering an operating temperature range from -55 °C to +125 °C, the SRN3010BTA Series is AEC-Q200 compliant and automotive grade. The features and design benefits delivered by these semi-shielded power inductors make them well-suited for automotive systems, DC-DC converters and power supplies in consumer, industrial, and telecom applications where higher inductor reliability is often required.

The Bourns® Model SRN3010BTA-330M semi-shielded power inductor is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf