Search
Languages

Bourns Adds New Model to Company’s Line of AEC-Q200 Compliant, Automotive Grade Semi-shielded Power Inductors

New Model SRN3010BTA-330M features high inductance value to optimize circuit performance and bottom-soldered lead-wire that enhances reliability

RIVERSIDE, Calif., March 12, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that it has added a new high inductance model to its SRN3010BTA Series Semi-shielded Power Inductors. The new Model SRN3010BTA-330M features an inductance value of 33 microhenries (µH) for efficient current handling. Its bottom-soldered lead-wire offers increased mechanical strength and stability for enhanced product reliability.

This power inductor model’s 1 mm max. profile semi-shielded structure combines the features of non-shielded and shielded inductors, providing lower magnetic field radiation than non-shielded inductors, and is considered a more cost-effective alternative to fully-shielded ferrite-based inductors. Offering an operating temperature range from -55 °C to +125 °C, the SRN3010BTA Series is AEC-Q200 compliant and automotive grade. The features and design benefits delivered by these semi-shielded power inductors make them well-suited for automotive systems, DC-DC converters and power supplies in consumer, industrial, and telecom applications where higher inductor reliability is often required.

The Bourns® Model SRN3010BTA-330M semi-shielded power inductor is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com