Search
Languages

Bourns® High-Voltage, High-Energy GDT Series Offers Industry-Leading Surge Protection Performance in a Compact Package

UL Recognized, the new GDT225HE Series meets the reliability requirements of lightning-prone industrial, renewable energy and telecom applications

RIVERSIDE, Calif., February 24, 2026  - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its GDT225HE Series High Voltage, High Energy Gas Discharge Tube (GDT) Arresters. Providing industry-leading surge protection performance in a compact package, Bourns® new GDTs are optimized for high-energy AC-DC power systems, including EV charging infrastructure, Battery Energy Storage Systems (BESS) and industrial power conversion equipment. These systems, in particular, are known to experience commutation or fault insertion events. It is the series’ ability to safely conduct prolonged high thermal (I²t) energy during transient conditions that makes it well-suited for system-level surge and fault protection, equipotential bonding and for lightning-prone designs where high-energy discharge must be safely diverted and controlled.

The Bourns® GDT225HE Series features a broad DC Breakdown Voltage (DCBV) from 1000 to 2000 V, In 40 kA (Nominal Discharge Current) and Imax 60 kA (Maximum Discharge Current) ratings on an 8/20 μs waveform to deliver exceptional protection for lightning-prone and high-energy applications. These high-power GDTs provide a space-saving alternative to bulky surge protection solutions by delivering very high current handling capabilities for AC power line applications in a small low-profile, reduced-volume and space-saving footprint. To help designers satisfy the requirements in today’s high-density and space-constrained PCB-based designs, this new series is also available in various lead shapes to fit in different configuration specifications.

The Bourns® GDT225HE Series is available now and is UL Recognized, ITU-T K.12 tested and RoHS compliant*. For additional information, please see: bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/high-voltage-series.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf