Search
Languages

Bourns Latest RF Inductors Deliver High Reliability from Advanced Multilayer Technology and Monolithic Construction

The four new multilayer chip inductor series are optimized for RF applications and deliver high-frequency performance with a compact, low‑profile design

RIVERSIDE, Calif., February 23, 2026 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced four Multilayer Chip Inductor Series: the CE0603G, CE0603M, CE1005Q, and CE1608Q Series. These new inductors feature a monolithic structure achieved through advanced multilayer technology giving power electronics designers a high-reliability, stable and superior signal integrity solution. These four series are available in compact form factors ranging from 1608 and 1005 down to the smallest 0603 mm, providing designers with more options in smaller sizes.

Helping to enable enhanced performance in high-frequency circuits, the new chip inductors feature high Self-Resonant Frequency (SRF) values of up to 20,000 MHz with tight inductance tolerance and rated current values from 100 to 1000 mA. All four high-SRF inductor series feature an operating temperature range from -55 to +125 °C, and have been optimized for use in RF amplifiers, low-voltage power supply modules, radio transmitters, radar, wireless communication and various mobile electronic devices.

Bourns® CE0603G, CE0603M, CE1005Q, and CE1608Q Series Multilayer Chip Inductors are available now and are RoHS compliant*. For more detailed product information, please see: bourns.com/products/magnetic-products/chip-inductors-multilayer.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf