Search
Languages

Bourns Introduces Shielded Power Inductor Series Designed with Carbonyl Powder Core Delivering High Saturation Current Capability

SRP4020T Series features a high heating current rating and shielded construction, offering low magnetic field radiation that meets power electronics efficiency/performance needs

RIVERSIDE, Calif., July 24, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its SRP4020T Series Shielded Power Inductors. This series features an advanced carbonyl powder core that offers excellent thermal stability and magnetic performance, making it suitable for demanding environments. Its shielded construction effectively suppresses magnetic interference and enhances Electromagnetic Compatibility (EMC).

Offered in a compact (4.45 x 4.0), low-profile (1.8 mm) package, the SRP4020T Series supports operating temperatures up to +150 °C, making it ideal for space-constrained designs. The inductance range for this series is from 0.47 to 10 μH. Compared to other similarly sized shielded inductors, it offers lower DC resistance (DCR), which helps reduce power losses and improve overall system efficiency. The SRP4020T Series is well-suited for consumer electronics and various power supply applications.

The Bourns® SRP4020T Series is available now through Bourns’ authorized distribution partners, and is RoHS* compliant. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf