Search
Languages

Bourns Adds Four New Product Series to its Shielded Power Inductor Portfolio

New shielded power inductors feature high heating/saturation current and low magnetic field radiation

RIVERSIDE, Calif., April 29, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today added four new product series to its line of shielded power inductors. The Bourns® SRP4021HMCT, SRP4021HMT, SRP5030HMCT, and SRP5030HMT Shielded Power Inductor Series feature high heating and saturation current with low magnetic field radiation to deliver enhanced power handling, increased efficiency, and optimized power circuit filtering.

The new shielded power inductors are produced with a hot press molding process that matches design needs for inductive components with greater density and additional mechanical strength. Compared to the previous Bourns® SRP series, the electrical characteristics have been enhanced by approximately 20 percent. This improvement is reflected in parameters such as the series’ higher current rating, lower DCR, and reduced power loss. The result is that Bourns is able to offer a smaller size inductive solution while maintaining the same electrical performance.

The Bourns® SRP4021HMCT, SRP4021HMT, SRP5030HMCT and SRP5030HMT Shielded Power Inductor Series are available now from Bourns’ authorized distribution partners, and are RoHS* compliant. For more detailed product information, please see: /bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf