Search
Languages

Bourns Introduces New Powerful, Ultra-Compact Gas Discharge Tube (GDT) Surge Protection Device Series

The industry-leading transient voltage protection features in the Bourns® Model GDT21 Series provide an advanced level of surge defense for space-sensitive industrial and communication applications

RIVERSIDE, Calif., December 3, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new powerful, ultra-compact Gas Discharge Tube (GDT) series. The products offered in the Bourns® Model GDT21 Series are 2-electrode devices that are designed to provide maximum impulse voltage limiting in a space-saving surface mount package. Bourns specifically engineered this new series to meet the requirements of space-constrained applications that now need more advanced protection against induced voltage transients, such as lightning and AC switching loads.

The Bourns® Model GDT21 Series is offered in a compact EIA 1206 package, and features industry-leading surge protection capabilities that help ensure reliable performance in demanding environments. The series’ advanced voltage limiting with quick response times aids in minimizing stress on downstream components during fast-rising transient events. In addition, the Bourns® Model GDT21 Series has a wide operating temperature range from -40 °C to +105 °C and a voltage range from 150 V to 600 V. The series provides very low capacitance for minimal insertion loss, making it ideal for maintaining signal integrity in communication systems, as well as for industrial controls, set-top boxes, HVAC systems, antennae, and many more designs.

“The launch of our Model GDT21 Series showcases Bourns' commitment to expanding our high-performance circuit protection offering in miniature form factors,” said David Chavarría, GDT/SPD Product Line Manager at Bourns. “By collaborating closely with our customers, Bourns continues to respond to evolving application needs for superior surge handling, high reliability, and space-efficient solutions. I’m pleased to announce that our new Model GDT21 Series successfully meets these demanding require-ments.”

Bourns® Model GDT21 Series is available now and is RoHS compliant* and UL recognized. For additional product information, please see: www.bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/standard-surface-mount-(smd)-2-electrode.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf