Leave a message
MENU
Search
Languages

Bourns Introduces New Powerful, Ultra-Compact Gas Discharge Tube (GDT) Surge Protection Device Series

The industry-leading transient voltage protection features in the Bourns® Model GDT21 Series provide an advanced level of surge defense for space-sensitive industrial and communication applications

RIVERSIDE, Calif., December 3, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new powerful, ultra-compact Gas Discharge Tube (GDT) series. The products offered in the Bourns® Model GDT21 Series are 2-electrode devices that are designed to provide maximum impulse voltage limiting in a space-saving surface mount package. Bourns specifically engineered this new series to meet the requirements of space-constrained applications that now need more advanced protection against induced voltage transients, such as lightning and AC switching loads.

The Bourns® Model GDT21 Series is offered in a compact EIA 1206 package, and features industry-leading surge protection capabilities that help ensure reliable performance in demanding environments. The series’ advanced voltage limiting with quick response times aids in minimizing stress on downstream components during fast-rising transient events. In addition, the Bourns® Model GDT21 Series has a wide operating temperature range from -40 °C to +105 °C and a voltage range from 150 V to 600 V. The series provides very low capacitance for minimal insertion loss, making it ideal for maintaining signal integrity in communication systems, as well as for industrial controls, set-top boxes, HVAC systems, antennae, and many more designs.

“The launch of our Model GDT21 Series showcases Bourns' commitment to expanding our high-performance circuit protection offering in miniature form factors,” said David Chavarría, GDT/SPD Product Line Manager at Bourns. “By collaborating closely with our customers, Bourns continues to respond to evolving application needs for superior surge handling, high reliability, and space-efficient solutions. I’m pleased to announce that our new Model GDT21 Series successfully meets these demanding require-ments.”

Bourns® Model GDT21 Series is available now and is RoHS compliant* and UL recognized. For additional product information, please see: www.bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/standard-surface-mount-(smd)-2-electrode.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.