Search
Languages

Bourns Releases Low-Profile Shielded Power Inductor Series Featuring Low DCR with Flat Wire

The nine models in the Bourns® Model SRP-F Series offer high heating/saturation current and low radiation in a small form factor

RIVERSIDE, Calif., November 6, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released its Model SRP-F Series shielded power inductors. The nine models in the series feature low DCR with flat wire construction in a small, low-profile (0.7 to 1.0 mm) form factor. The flat wire construction improves the efficiency of these new power inductors by significantly reducing DCR compared to other similarly sized power inductor devices that use conventional wire.

The models in the SRP-F Series are designed with a metal alloy powder core, flat wire technology and advanced molding technology to achieve a higher saturation current and heating current level with low radiation in a small form factor. The series delivers a low buzz noise solution with an inductance range of 0.3 - 10 µH and an operating temperature range of –40 to +125 °C. These features are required in a growing variety of space-constrained applications that require high current, but must also meet lower power consumption goals, such as in consumer, industrial, and telecom application DC-DC converters and power supplies.

The Bourns® Model SRP-F Shielded Power Inductor Series is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf