Bourns Releases Low-Profile Shielded Power Inductor Series Featuring Low DCR with Flat Wire

The nine models in the Bourns® Model SRP-F Series offer high heating/saturation current and low radiation in a small form factor

RIVERSIDE, Calif., November 6, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released its Model SRP-F Series shielded power inductors. The nine models in the series feature low DCR with flat wire construction in a small, low-profile (0.7 to 1.0 mm) form factor. The flat wire construction improves the efficiency of these new power inductors by significantly reducing DCR compared to other similarly sized power inductor devices that use conventional wire.

The models in the SRP-F Series are designed with a metal alloy powder core, flat wire technology and advanced molding technology to achieve a higher saturation current and heating current level with low radiation in a small form factor. The series delivers a low buzz noise solution with an inductance range of 0.3 - 10 µH and an operating temperature range of –40 to +125 °C. These features are required in a growing variety of space-constrained applications that require high current, but must also meet lower power consumption goals, such as in consumer, industrial, and telecom application DC-DC converters and power supplies.

The Bourns® Model SRP-F Shielded Power Inductor Series is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.