Search
Languages

Bourns Expands Shielded Power Inductor Portfolio with New Dual-Winding Series

Bourns® Model SRF3015 Series offers a cost-effective, space saving solution in a low 1.4 mm profile design

RIVERSIDE, Calif., October 28, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new cost-effective, space saving dual-winding shielded power inductor series. Bourns® Model SRF3015 Series features a low profile of 1.4 mm and shielded construction that provides low radiation making these inductors optimal solutions for attenuating high frequency noise in a broad range of circuits.

Bourns® latest power inductors offer an extended operating temperature range of -40 °C to +125 °C, and are particularly well-suited for use in SEPIC (Single-Ended Primary Inductance Converter) topologies and power supplies.

The Bourns® Model SRF3015 Series dual-winding shielded power inductors are available now, and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chokeswww.bourns.com/products/magnetic-products/power-inductors-smd-dual-winding-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf