Search
Languages

Bourns Announces Zero Ohm High Power Jumper Resistor Series Offering Very Low Resistance Values

Featuring a high current rating and a robust metal strip element, Bourns® AEC-Q200 compliant jumpers enable designers to connect separated points on a PCB

RIVERSIDE, Calif., January 29, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the Model CRF Series High Power Metal Strip Jumper. Also known as zero ohm resistors, jumpers feature very low resistance values, and are used to connect separated points that cannot be connected via printed traces on a PCB. Compared to thick film jumpers, Bourns' new AEC-Q200 compliant high power jumpers offer a higher current rating and lower resistance, making them well-suited for broad range of consumer, industrial, telecommunication and automotive designs.

Bourns® new Model CRF Series zero ohm jumpers are manufactured using copper alloy with a protective overcoat material, and are offered in four different footprint sizes; 0805, 1206, 2010 and 2512, and provide a maximum resistance value of 0.2 milliohms. They feature a high current rating up to 100 A, an operating temperature range of -55 °C to +150 °C and are available in tape and reel packaging.

The Bourns® Model CRF Series high power metal strip jumper is available now. These models are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/resistors/fixed-resistors-aec-q200-compliant-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf