Search
Languages

Bourns Launches Automotive Grade Semi-shielded Power Inductor Series Featuring High Operating Temperatures Up to 150 °C

AEC-Q200 compliant inductor series is constructed with magnetic silicon-based coating technology for superior magnetic shielding and supports higher operating temperatures

RIVERSIDE, Calif., June 22, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new AEC-Q200 compliant, automotive grade semi-shielded power inductor series that features a high operating temperature range from -40 °C up to 150 °C. The Bourns® Model SRN8040HA Series is constructed using the company's advanced magnetic silicon-based coating technology that offers superior magnetic shielding while also enabling higher operating temperatures.

Bourns' new high temperature inductors are designed to release lower magnetic field radiation compared to non-shielded inductors, and are also a more cost-efficient alternative to fully shielded ferrite-based inductors. The Model SRN8040HA series supports high current capacity with saturation current Isat ranging from 1.3 – 15 A and provides a heating current Irms range of 1.0 – 10.0 A. The features and capabilities of these inductors make them especially well-suited for DC-DC converters and power supplies in automotive, consumer, industrial, and telecom electronics applications where greater inductor reliability is a frequent requirement.

The Bourns® Model SRN8040HA semi-shielded power inductor series is available now and is RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-semi-shielded/product/SRN8040HA

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf