Search
Languages

Bourns Announces Five Shielded Power Bead Inductor Series Featuring High Rated Current with Extremely Low DC Resistance

Bourns® Model SPB inductors are designed to enhance efficiency, reduce power losses in multi-phase integration applications

RIVERSIDE, Calif., November 1, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced five new shielded power bead inductor series that feature high rated current, ferrite-based shielded construction and extremely low DC resistance from 72 to 440 nH. Bourns designed the new Model SPB0705, SPB1005, SPB1007, SPB1012 and SPB1308 series to match the enhanced efficiency, low magnetic field radiation and reduced power loss requirements in a broad variety of multi-phase integration applications.

The advanced features and the multiple SMD footprints (6.7 x 6.5 to 13.5 x 13 mm) offered in the five new power inductor series make them excellent power conversion solutions for applications in Voltage Regulator Modules (VRMs), power processors, memory modules, high current ASICs, servers, storage, data centers, networking systems and graphic cards.

All five of the new Bourns® Model SPB0705, SPB1005, SPB1007, SPB1012 and SPB1308 inductor series are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/power-inductors-smd-shielded

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf