Search
Languages

Bourns Announces New Non-Contacting Feedback Rotary Sensor with SSI Output

New Model DMS22B is designed to meet heavy-duty application specifications for long cycle life and high reliability

RIVERSIDE, Calif., May 3, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced its latest non-contacting feedback rotary sensor that features Synchronous Serial Interface (SSI) output providing effective synchronization in closed-loop control systems. This single-turn rotary sensor is based on Hall Effect technology and is supported by a factory programmable electrical angle from 10 to 360 degrees that enables more consistent and dependable operation of up to 50 million shaft revolutions.

The Bourns® Model DMS22B rotary sensor is designed with non-contacting magnetic technology offering consistent excellent performance and high reliability that is well-suited for a range of application environments. Plus, its IP50 seal rating makes this rotary sensor highly resistant to fluid/dust ingress. Available with a 7/8-inch flatted shaft and bushing mount configuration, the Bourns® Model DMS22B rotary sensor offers designers a highly versatile position sensing solution for a broad variety of applications including patient platform positioning feedback, pneumatic control valve position feedback, draw wire position sensors, remote communications antenna positioning, actuator motor position feedback, automated manufacturing robotics and more.

The Bourns® Model DMS22B rotary sensor is available now and is RoHS* compliant. For more detailed product information, please see: www.bourns.com/products/sensors/position-sensors/non-contacting-single-turn

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf