Search
Languages

Bourns Further Expands its Discrete TVS Diode Product Line

RIVERSIDE, Calif., October 21, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the further expansion of its industry-leading line of discrete transient voltage suppressor (TVS) diode products with two new series of ESD/EFT surge protection products. Bourns designed its Model SMA6J and Model SMA6J-Q TVS diodes to protect power buses and I/O interfaces in data lines and DC power supplies. In addition, Bourns® Model SMA6J-Q is AEC-Q101 compliant and well-suited for a broad range of communications, industrial and consumer electronics applications that are used in certain harsh environments and require high reliability.

Both model series come in a compact, industry standard DO214-AC (SMA) package, and feature increased peak pulse power (PPP) dissipation of 600 watts compared to the 400-watt industry standard. TVS diodes are typically rated for peak pulse power allowing designers to determine the best type required for a particular application and environment. These unidirectional/bidirectional devices offer reverse standoff voltage of 5 – 43 V. The features of Bourns' new TVS diodes help enable power supply designers to meet their both their high-power density and small form factor requirements.

Bourns® Models SMA6J and SMA6J-Q are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/diodes/diodes-aec-q101-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf