Search
Languages

Bourns Announces New High Current Surge Device Designed for SLIC Overvoltage Protection

Riverside, Calif., October 22, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the release of its new high current surge devices designed to protect SLICs (Subscriber Line Interface Circuits) against overvoltage conditions on the telephone line caused by lightning, a.c. power contact and induction. The dual programmable Thyristor overvoltage device, designated Bourns® Model TISP61089M, is a high-surge current protector rated at 70 A for a 5/310 surge. It limits voltages that exceed the SLIC supply rail voltage, and is specified to support equipment compliance with transient immunity and Electromagnetic Compatibility (EMC) Bellcore GR-1089-CORE, ITU-T K.21 and K.45 and YD/T-950 standards.

To provide optimum protection during Metallic (Differential) and Longitudinal (Common Mode) surge conditions, Bourns’ latest high current surge device features two negative protection structures and two anti-parallel diodes. For SLIC line driver sections that are typically powered from 0 V (ground) and a negative voltage (from -20 V to -155 V), Bourns’ new overvoltage device supports a negative supply voltage down to -155 V and requires a low gate triggering current of 5 mA maximum. The buffered gate design reduces the loading on the SLIC supply during overvoltages caused by power cross and induction. In addition, Bourns fabricates its monolithic protection devices in ion-implanted planar vertical power structures for high reliability and in normal system operation they are virtually transparent.

The Bourns® Model TISP61089M is available now, and is packaged in a RoHS compliant* 8-SOIC package. As a pricing reference, the new dual programmable Thyristor overvoltage device is priced from $0.80 per 10,000-piece order. For detailed information, please go to: https://www.bourns.com/en/docs/product-datasheets/TISP61089M.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf