MENU
Search
Languages

Bourns Adds 19 New Documents to its Successful PortNote® Solutions Series

Riverside, Calif., November 29, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that it has added 19 new PortNote® Solutions to assist designers in selecting the appropriate circuit protection solution for a specific port interface. These new documents add to the company's successful series that provide engineers with a simplified design starting point that includes precise information on relevant compliance standards, the optimal Bourns solution with part numbers, an interface schematic and alternative solution references. These new documents cover port protection for audio/video, battery pack, data communication, LED and telecommunications designs, and are a useful resource to help streamline the circuit protection selection process for a specific port interface. In addition to the documentation, Bourns offers corresponding design kits for each of the new PortNote® Solutions.

"We have seen an overwhelmingly positive response in the marketplace to Bourns' PortNote® Solutions series mostly due to how these documents can help customers reduce their circuit protection development time," said Dr. Erik Meijer, vice president of circuit protection at Bourns. "Circuit protection products are often designed into variations of interface ports and Bourns is committed to helping OEMs select the right solution for this sometimes difficult task. This documentation series is another example of the resources we can offer our customers in addition to our extensive experience and broad offering of circuit protection solutions."

The 19 new PortNote® Solutions offer protection information for LVDS input and output ports for audio/video applications; ESD protection for battery pack applications; Ethernet and RS-485 ports for datacom applications; PWM ports for LED applications and T1/E1 telephony, VDSL line side and VDSL over POTs for ports in telecom designs. The corresponding design kits contain sufficient Bourns® products to prototype five of the circuits designated in the PortNote® Solution. Bourns® PortNote® Solutions are not intended to replace detailed application notes or the customized solutions provided by Bourns' FAE teams, but instead provide useful information in the circuit protection selection process for a specific port interface. A total of 30 individual Bourns® PortNote® Solutions are easily accessible on the Bourns website at: www.bourns.com/Library.aspx?name=PortNoteSolutions.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf