Search
Languages

Bourns Releases New Power Terminations for RF Applications

Riverside, California, August 2, 2005 - Bourns is pleased to announce the release of a line of high frequency power resistors and terminations. Designated the CHF Series, these lightweight resistors are suitable for use in RF and microwave applications.

Package styles include chip, surface mount and flanged. This series is suited for a range of RF and Microwave applications including high power amplifiers, isolators, Wilkinson combiners, Power Dividers and Absorptive Filters. Construction material consists of either an aluminum nitride or beryllium body with a proprietary resistor element. The devices are optimized for 50 ohm characteristic impedance using special manufacturing techniques to reduce VSWR (voltage standing wave ratio). Power ratings range from 10 W to 250 W with a low return loss up to 4 GHz.

The pricing for the surface mount chips ranges from 0.7 USD to 1.20 USD depending on the size and power rating for a quantity of 10K pieces.

Product data sheets and an application note are available on the Bourns website at www.bourns.com.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf